Summary
Summary provides a brief account about the deviation of different parameters for the same systems.
To view Summary data for the selected system, click Summary tab.
Summary
Following table describes the various fields in the Summary tab:
|
Field Name |
Description/ Action |
|
Curve Name |
Name of the curve configured with the parameter. |
|
Nominal Value |
The latest reference value calculated based on the Nominal curve |
|
Nominal Value Deviation |
The deviation is calculated using the formula Nominal Deviation=(Process Value-Nominal Curve Value)/(Nominal Curve Value)*100 |
|
Parameter Name |
Name of the selected parameter. |
|
Process Value |
The actual value against the parameter. |
|
Reference Value |
Value of curve plotted based on the linear interpolation of Z axis curves based on actual operation. |
|
Reference Value Deviation |
The deviation is calculated using the formula Reference Deviation=(Process Value-Reference Value)/(Reference Value)*100 |