Link

The Link feature provides a quick-view option that allows you to navigate from a widget to another dashboard or a data-driven widget template.

Link to Another Dashboard

Use this option to link a widget to another dashboard. Configure this option in the Dashboard tab.

 Links Tab - Dashboard

Configuration Options

The following configuration options are available on the Dashboard tab:

Option

Description

Select target dashboard

Select a dashboard from the dropdown list to link it with the widget. The list displays all dashboards saved in the application.

After configuration, clicking the widget opens the selected dashboard.

Display Link As

Enable any one of the radio buttons to define how the linked dashboard is displayed.

  • Overlay: When enabled, clicking the widget displays the linked dashboard as an overlay on the current dashboard. You can close the overlay by clicking the X icon or pressing the Esc key.

  • Dashboard: When enabled, clicking the widget displays the linked dashboard in full view. You can use the Back button to return to the previous dashboard.

Data to be Passed

The attributes that are passed as data are used to drill to functionality for the given links. In the Param Value field, you can either manually enter the value or click the + icon to generate the Parameter Value Configuration pop-up and select the value.

For more information, see Variable Usage.

Link template with Data-Driven Model

Use this option to link a widget to another widget template based on a data-driven model. Configure this option in the Data-driven tab.

 Links Tab - Data-Driven

Configuration Options

The following configuration options are available on the Data-driven tab:

Option

Description

Model

Select the model from the dropdown.

Type

Select the type from the dropdown.

Template

Select the template to associate with the widget. When you click the widget, the selected template opens.

Display Link As

Enable any one of the radio buttons to define how the linked dashboard is displayed.

  • Overlay: When enabled, clicking the widget displays the linked dashboard as an overlay on the current dashboard. You can close the overlay by clicking the X icon or pressing the Esc key.

  • Dashboard: When enabled, clicking the widget displays the linked dashboard in full view. You can use the Back button to return to the previous dashboard.

Data to be Passed

The attributes that are passed as data are used to drill to functionality for the given links. In the Param Value field, you can either manually enter the value or click the + icon to generate the Parameter Value Configuration pop-up and select the value.

For more information, see Variable Usage.